Stability Calculation for TLS4125
A small-signal linearized model of the converter to predict the loop gain under varying
conditions.
Such as: input voltage, output current and external components
- Define output voltage variant and electrical parameters
- Click on „AC-sweep“ to view Simulation results
- Want more variations? Change circuit configuration
- Click on 'Hold result' to keep trace & compare to other Simulation results
Need support?
Technical Assistance
Technical Assistance
The simulation settings include switching frequency, input voltage, output voltage variant, output
voltage, output current, output capacitor, output capacitor esr and the inductor size. Results are
shown in the scope window. Additionally, the user can compare the effect of parameter and part
variations by holding different results. Be sure to take a look at the recommended external parts
for this product in the datasheet first. For certain combinations it is possible that no
cross-over of the magnitude plot with the 0 dB line occurs.