Stability Calculation for TLE927x Boost Converter
- Define output voltage variant and electrical parameters, select parts
- Click on „Steady-State“ to view Simulation results
- Want more variations? Change circuit configuration
- Click on 'Hold result' to keep trace & compare to other Simulation results
Need support?
Technical Assistance
Technical Assistance
The simulation settings include switching frequency, input voltage, output voltage, output
current, output capacitance and inductance. The results are shown in the scope window.
Additionally, the user can compare the effect of parameter variations by holding different
results. Be sure to take a look at the recommended external parts for this product in the
datasheet first. For certain combinations it is possible that no cross-over of the magnitude plot
with the 0 dB line occurs. Loop gain prediction is only valid for operation in continuous
conduction mode (CCM), so make sure that the converters’ output current is higher as the minimum
current needed to be in CCM (Imin_ccm).